How can I write protect sectors of internal flash (LPC1769)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I write protect sectors of internal flash (LPC1769)?

1,526件の閲覧回数
stenlarsson
Contributor II

I want to protect one or a few 4K internal flash sectors from being erased by the application (on purpose or by mistake). 

Is this possible?

0 件の賞賛
返信
2 返答(返信)

1,436件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Sten Larsson,

   Unfortunately, the LPC1769 hardware still can't support the flash protection function now.

 

 


Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,436件の閲覧回数
converse
Senior Contributor V

You cannot protect individual sectors

0 件の賞賛
返信