How can I debug a LPC810 prg using the little LPC800 board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I debug a LPC810 prg using the little LPC800 board?

1,349 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DG4EK on Tue Jul 02 20:09:29 MST 2013
Hi,
I just got started trying the small LPC800 board.
Uploading .hex files works perfect but I'm wondering
how to debug a program using LPCXpresso .?

When I use the debug button I'll get an error
saying "No compatible emulators available".

I guess I need additional hardware to connect to
the 10-pin plug? What additional hardware/software
do I need?

Thanks a lot for helping a beginner.
Labels (1)
0 Kudos
Reply
4 Replies

1,274 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Jul 05 07:41:23 MST 2013

As you say you are using LPCXpresso, you may find the LPCXpresso forum as useful place to look for help. In particular this recent thread may be of interest...


http://knowledgebase.nxp.com/showthread.php?t=4730


To actually debug an LPC810 with LPCXpresso though, you will basically need either an LPC-Link (from an LPCXPresso board), or an LPC-Link2.

0 Kudos
Reply

1,274 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leon_heller on Thu Jul 04 08:42:18 MST 2013

It's the LPC800 Mini-kit:


http://lpcware.com/lpc800-mini-kit

0 Kudos
Reply

1,274 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by starblue on Thu Jul 04 01:16:14 MST 2013
Which board do you mean by "small LPC800 board"?
0 Kudos
Reply

1,274 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leon_heller on Wed Jul 03 08:59:10 MST 2013

You need a suitable JTAG/SWD interface. I used a Rowley CrossConnect with the SWD adapter with their CrossWorks compiler and debugger.

0 Kudos
Reply