How accurate is the NXP LPC546XX temperature sensor?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How accurate is the NXP LPC546XX temperature sensor?

1,019件の閲覧回数
lukea
Contributor I

Hi,

The NXP LPC546xx  datasheet has the below text in section 7.2.2 Temperature sensor:

        The output voltage varies inversely with device temperature with an absolute accuracy of better than ±5 deg C over the full temperature range (-40 deg C to +105 deg C).
        The temperature sensor is only approximately linear with a slight curvature.
        The output voltage is measured over different ranges of temperatures and fit with linear-least-square lines.

But also in section 12.3 (Temperature sensor as well) there is a table that shows accuracy as Max 3.7 Degrees C.
Does anyone know which is correct?
Or is it a case of linearity error on top of +/- 5 Deg C making it +/- 8.7 Deg C?

lukea_0-1702424291646.pnglukea_0-1702424291646.png

Thank you

Luke




 

0 件の賞賛
返信
1 返信

1,004件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that we get the slop and offset after Linear-Least-Square (LLS) fit, the m is -2.05, the offset is 584.

This is the formula to figure out the temperature:

sensor output voltage=-2.4mv/Degree*temperature+584mV

With above formula, we can guarantee that the error is less than 3.7 degree in the -40 to +105 degree range.

Hope it can help you

BR

Xiangjun Rong

0 件の賞賛
返信