How To make a plain load image with M0 cores

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How To make a plain load image with M0 cores

2,295件の閲覧回数
zhengyangqu
Contributor II

LPC43S70 can load AES encrypted image from QSPI flash using SPIFI.

The problem is, images of M0 cores cannot be copied to right position so that M0 cores cannot boot up correctly, while the M4 core works just fine.

plus, Normal image(XIP in QSPI flash) can boot up correctly.

Help wanted.

Memory map:

M4: use Plain Load Image option, addr: 0x1000_0000

M0APP addr: 0x2000_0000

M0SUB addr: 0x1800_0000

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,141件の閲覧回数
zhengyangqu
Contributor II

I have already implement boot all of the three cores from spifi flash.

0 件の賞賛
返信

2,141件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Zhengyang Qu,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I'd highly recommend you to directly debug the dual-core demo in the RAM as the first step to the implementing the secure boot, as it can give you some clues about the 'issue', please give a try.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信