How To Create CFPA Page Binary

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How To Create CFPA Page Binary

2,215 Views
tuline
Contributor I

Hello,

I've been going over the steps in AN12283, and I'm a little confused on the steps needed to generate a binary file that can be loaded into the CFPA flash region. The application note says there is an example attached (referenced in section 5.4), but I don't see any way to access an attachment. I'm hoping someone can point to the right documentation on how to construct the appropriate CMPA/CFPA binaries for working with signed image or at least provided a rough overview on how to about it. Apologies if I'm just misreading the application note, if that's the case just point me at the appropriate section and I'll give it a closer read. 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,107 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Ben

I have attached the AN12283 referred attachment. I hope this can help you understand the CFPA page programming.

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply