How I set up the LPC-Link2 for LPC4313 programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How I set up the LPC-Link2 for LPC4313 programming

2,183 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by haber on Sun Feb 21 11:13:41 MST 2016
Hi.

I'm trying to upload some program on LPC4313(LQFP144, no devboard) using LPC-Link2.

I'm using LPCXpresso 8.0.0 IDE and JTAG/SWD pin J6 on LPC-Link2.

In this situation,

1. should I short J1 on LPC-Link2?

2. What pin is the main power on LPC4313? (VDD(VDDA, VBAT), VSS(VSSIO) is right?)

3.Is it right to set up the emulator selection in debugger configuration as CMISIS-DAP?

4. What LPC-Link2 firmware is right(In LPC-Link2 Configurarion Tool)?

When I set up the debugger connection in debugger configuration as JTAG with CMISIS-DAP emulator

and debug, 'JTAG configuration - No available devices found' error occured.   

How should I set up the configuration LPC-Link2, LPCXpresso IDE for uploading program on a LPC4313?

Thank you.
Labels (1)
0 Kudos
Reply
4 Replies

2,124 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by haber on Sat Feb 27 10:20:37 MST 2016
Thanks for your reply.

Yeah. I thinks so too.

When I attempt to connect JTAG with J6 of LPC-Link2, LPCXpresso can't connect to the core.

But, When I connect JTAG with J7(10 pin IDE connect), I succeed in debugging LPC4313 core.

I think that 3.3V VTref connection is the key point.

Because the difference between successful case and the other is only 3.3V power(VTref) connection. 

When I connect the core using J6, I use 3.3V power with first pin in J6.

Thanks for you again.

Thank you.
0 Kudos
Reply

2,124 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Wed Feb 24 01:56:16 MST 2016

Quote:
What's the matter?


Given the very little information you have provided, it is diffuclt to say, but I would start by looking at power.
0 Kudos
Reply

2,124 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by haber on Wed Feb 24 01:08:03 MST 2016
First of all, thanks for your reply.

I understand what you saying, and I set up the LPCXpresso IDE and LPC-Link2 debugger tool.

And I designed rightly SWD/JTAG pull-up/pull-down resistor referring to site(https://www.lpcware.com/content/faq/lpcxpresso/debug-desig).

But, I can't still connect LPC4313 core using JTAG or SWD.

On the other hand, I succeed  in debugging with LPC4088 core.

I use same debugging tool and SWD/JTAG circuit design.

I will use IRC(12Mhz internal clock) in LPC4313, so I don't connect any XTAL, RTCX. Is it matter?

I have been attempted debug with two LPC 4313 core, one LPC 4330 core, but all attempt failed to connect.

What's the matter?

Thank you.
0 Kudos
Reply

2,124 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Feb 22 01:40:15 MST 2016
If you leave JP1 open, then the LPCXpresso IDE will soft-load appropriate probe firmware into your LPC-Link2 the first time you debug after powering up.

If you really want to pre-program the firmware into your LPC-Link2, then use LPCScrypt - as described in:

[list]
  [*]https://www.lpcware.com/content/faq/lpcxpresso/lpc-link2-debug-probe-firmware-programming
[/list]

In 99.99% of cases, there is no need to manually select setting yourself in the launch configurations, as LPCXpresso IDE will automatically generate the required settings based on the probe it auto-detects in your system. Please read the supplied documentation for more details.

For details on how to connect debug related signals, please see:

[list]
  [*]https://www.lpcware.com/content/faq/lpcxpresso/debug-design
[/list]

PS - you might want to watch some of our introductory videos on using LPCXpresso IDE....

[list]
  [*]https://www.youtube.com/watch?v=NW7GmsMcrKc
  [*]https://www.youtube.com/watch?v=IIF8A8A_CGA
[/list]

Regards,
LPCXpresso Support
0 Kudos
Reply