High Speed MOSFET Driving with GPIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

High Speed MOSFET Driving with GPIO

3,736 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by neilt6 on Thu Jun 20 12:36:33 MST 2013

Hey guys. I'm trying to build a high-speed push-pull driver using a P-channel and N-channel MOSFET connected to a PWM pin on an LPC11U35, but I'm having a little trouble with choosing a gate resistor. My understading is that the gate resistor limits the instantaneous current caused by the gate capacitance. According to the LPC11U35 datasheet, the GPIO pins are only rated for about 4mA (Actually it says -4mA and I have no idea why, if anybody could shed light on this as well that'd be great), so I've been using 1.5k gate resistors up until now. However, I need this push-pull driver to swtich between 500kHz to 1MHz. This is obviously not going to happen with a 1.5k resistor, the output just sits high all the time. What do I need to do to make this work?

Labels (1)
0 Kudos
Reply
4 Replies

3,678 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by neilt6 on Tue Jul 02 19:04:29 MST 2013
Ok, that makes sense. Turns out I had to redesign the whole circuit, and now I'm only switching one N-channel MOSFET at 1MHz. By dropping the gate resistor to 100Ω for a maximum instantaneous current if 33mA, I was able to get it to switch nicely. Thanks guys!
0 Kudos
Reply

3,678 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larsen on Fri Jun 21 13:02:40 MST 2013

you say the output is high all the time, but do not say if it is the gpio or the fet output. If it is the latter, then check if the gpio is able to pass the thresholds of the fets. If not, then no resistive gate resistor value can help. 


Also check if your gpio output is actually toggling when no fet's attached.


The 4mA will give you a slew rate of I/C = 4mA/(Cgatep+Cgaten). so for 1nF the slew rate would be 4V/us. Fets have fairly high gate capacitance. Check you own numbers - will it be able to swicth fast enough?

0 Kudos
Reply

3,678 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Thu Jun 20 15:11:56 MST 2013

The specification for the LPC11U35 defines a IOH=-4mA (VOH=VDD-0.4V) and IOL=4mA (VOL=0.4V).  If you don't mind your VOH and VOL values to have higher offsets from VDD and GND, then you can source/sink higher currents (see IOHS and IOLS parameters in the data sheet).  Figures 17 and 18 in the data sheet show how the current affects VOL and VOH.

0 Kudos
Reply

3,678 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leon_heller on Thu Jun 20 13:21:29 MST 2013

It's -4 mA because the pin sinks current. It would be positive if it sourced current.

0 Kudos
Reply