Hi,I am using 1pc1768 chip.It Working as a USBHID device.It Recognizes on system in the name"USB HID vendor defined device".I need to change the manufacturer name.Where should i change it?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi,I am using 1pc1768 chip.It Working as a USBHID device.It Recognizes on system in the name"USB HID vendor defined device".I need to change the manufacturer name.Where should i change it?

1,723件の閲覧回数
saravanans
Contributor I

We are working on USB HID lpc1768 board.HID device recognizes as "USB HID vendor defined device".We need to change a name from vendor defined device to some friendly name(Manufacturer name).Where should i change in Device descriptors in code.please help us.

0 件の賞賛
返信
2 返答(返信)

1,594件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please take a look to the following page for more information about the NXP USB VID program and how to apply for the NXP VID and get up to 3 FREE PIDs.
USB VID PID Program|NXP 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,594件の閲覧回数
saravanans
Contributor I

Hi

Thanks for the reply.

We have received our VID and PID from NXP.

We need to change the device string from the generic one (USB HID compliant Vendor defined device) to our device string. How can we do this ? any procedure to be followed or sample work available?

Thanks in Advance.

Regards

Saravanan

0 件の賞賛
返信