Hex file transfer back from device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hex file transfer back from device

2,299件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ssrli on Thu Oct 03 23:00:19 MST 2013
Hello,

I'm working on a small project using an NXP lpc1769 demo board. I'm using LPCExpresso 5 from CodeRed to program it and I would like to know if I can transfer the application hex/bin file back from the board to the PC.
Either with the IDE or with any other solution.

Thanks in advance, Adrian
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,253件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Oct 04 02:18:53 MST 2013
And now FAQ'ed with a couple of screenshots...

http://www.lpcware.com/content/faq/lpcxpresso/import-export-memory

Regards,
LPCXpresso Support
0 件の賞賛
返信

2,253件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Oct 04 01:50:58 MST 2013
Use the Export option in the Memory View. See this previous thread for details:

http://www.lpcware.com/content/forum/reading-dump-image-from-a-part-via-lpc-link

Regards,
LPCXpresso Support
0 件の賞賛
返信

2,253件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfbsoftware on Fri Oct 04 01:39:41 MST 2013
Connect your LPC1769's UART0 to a COM port on your PC and then you can use FlashMagic to transfer a range of locations to your PC as a HEX file. If you do not already have FlashMagic you can download it from:

http://www.flashmagictool.com
0 件の賞賛
返信