Help URGENT with error 15:target error from commit flash write: et: flash driver not ready

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help URGENT with error 15:target error from commit flash write: et: flash driver not ready

2,601 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pindonga123 on Thu Oct 31 12:19:39 MST 2013
Hello Im working with 1769 and i can't debug. This legend appear 15:target error from commit flash write: et: flash driver not ready
I do this Once you have managed to recover debug access to the MCU, the first thing that you should do is overwrite the image in flash with one that sets the system up in a safe manner, so that future debug connections will be successful without the need to recover debug access again. You would normally use the in-built flash programmer to erase the flash. but i couldn't understand the steps. Because i do this but dont work. Sorry but my english is very bad. When i wanna do a mass erase appear the next legend
Pc: (  0) Reading remote configuration
Ni: LPCXpresso Debug Driver v4.0 (May 21 2012 21:42:41)
Nc: Looked for chip XML file in C:/nxp/LPCXpresso_4.2.3_292/lpcxpresso/bin/LPC1769.xml

Nc: Looked for vendor directory XML file in C:/nxp/LPCXpresso_4.2.3_292/lpcxpresso/bin/nxp_directory.xml

Nc: Found generic directory XML file in C:/nxp/LPCXpresso_4.2.3_292/lpcxpresso/bin/crt_directory.xml

Pc: (  5) Remote configuration complete
Pc: ( 30) Emulator Connected
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: Emu(0): Conn&Reset. DpID: 2BA01477. Info: T1S6RGRIA
Nc: SWD Frequency: 250 KHz. RTCK: False. Vector catch: False.
Nc: Packet delay: 0  Poll delay: 0.
Nc: NXP: LPC1769  Part ID: 0x26113F37
Pc: ( 65) Chip Setup Complete
Nt: Connected: was_reset=true. was_stopped=false
Cr:v Registered license, download limit of 128K
Pc: ( 70) License Check Complete
Nt: Mass Erase
Ed:04: Failed to erase flash: Ef(9). Flash erase or write operation aborted.
Pc: (100) Target Connection Failed
What could be?
Labels (1)
0 Kudos
Reply
6 Replies

2,585 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Oct 31 13:06:48 MST 2013
Sorry, can't skype at work.
0 Kudos
Reply

2,585 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pindonga123 on Thu Oct 31 12:41:09 MST 2013
Can you agree me to skype?. [email protected]
0 Kudos
Reply

2,585 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Oct 31 12:37:04 MST 2013
Then switch to ISP (pull P2.10 low and reset):

http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip

And update LPCXpresso to Version6:

http://www.lpcware.com/content/forum/lpcxpresso-latest-release

0 Kudos
Reply

2,585 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pindonga123 on Thu Oct 31 12:35:05 MST 2013
Sorry but im seeing you online i wanna do a real time chat but i dont know how i can agree you like contact
0 Kudos
Reply

2,585 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pindonga123 on Thu Oct 31 12:32:49 MST 2013
I Could debug this board before.
It is a custom.
What do you mean ISP and Vector catch? I dont have de more minimal idea....ja ja. Sorry but Im new Programming MCU
I was using the same version the same software version after and before it broken
0 Kudos
Reply

2,585 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu Oct 31 12:27:15 MST 2013
Could you debug this board before?

Is it a custom board?

Did you try ISP and Vector catch?

Why do you use an old version instead LPCXpresso6? 
0 Kudos
Reply