He

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决
1,809 次查看
gouthamdugyala
Contributor I

Hi,

      I'm using LPC5410x NXP controller, we are implementing SPI FIFO-DMA full duplex mode. As of now we understand that SPI Tx register has 32-bit register(16-bit for control/16-bit for DATA) whereas SPI Rx register 32-bit register dedicated to DATA.

To work in full duplex mode, i configured the control register for MasterTx and its working fine. should i configure the same to SlaveTx??

Whether configure or not we are missing few bytes initially and duplication happening at end.

Please suggest how to handle SlaveTx data

Chethan

标记 (1)
0 项奖励
回复
1 解答
1,728 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi goutham dugyala,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
I'd highly recommend you to refer to the dma_transfer demo from the SDK of the LPC54102, this demo illustrates how to use spi driver with DMA and you can create the SDK via the link below.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,729 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi goutham dugyala,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
I'd highly recommend you to refer to the dma_transfer demo from the SDK of the LPC54102, this demo illustrates how to use spi driver with DMA and you can create the SDK via the link below.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复