Hardware IP checksum feature removed from ethernet block

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hardware IP checksum feature removed from ethernet block

1,412 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Johnny D on Wed Mar 19 04:23:05 MST 2014
Hi,

I was wondering if someone could explain this little line in the 43xx user manual?:
"Hardware IP checksum feature removed from ethernet block".

On all the (current) NXP web pages relating to the 43xx mcus, they state "10/100 Ethernet with hardware enabled TCP/IP checksum calculation". But they seem to have removed this feature.

So, will a 4357 do tcp/ip checksum calculations in hardware or not?

Many thanks,

John.
Labels (1)
0 Kudos
Reply
1 Reply

1,375 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Wed Mar 19 08:52:19 MST 2014
I don't understand. TCP/IP is a protocol on top of Ethernet.
How can the Ethernet hardware know about the TCP payload checksum (without having to know pretty much about TCP)?
0 Kudos
Reply