Hard floating point USBD library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hard floating point USBD library

2,014 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by npeterson on Mon Sep 14 11:10:09 MST 2015
We are using a LPC4078 controller in a product and would like to investigate using the the Hard ABI FPU to see if there is a performance benefit. Unfortunately it looks like there is not a version of the precompiled USB library that is part of LPCOpen that has support for the FPU configured with Hard ABI.

Is there a version of libusbd_40xx_lib.a that will work with projects that are configured to use Hard ABI?
Labels (1)
0 Kudos
Reply
3 Replies

1,949 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Support on Tue Oct 27 11:45:00 MST 2015
Hi npeterson,

Sorry for the delay - I attached the hard ABI USBD library file for LPC4078. 

Best regards,
-NXP Support
0 Kudos
Reply

1,949 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by npeterson on Mon Oct 05 17:58:55 MST 2015
We are using LPCXpresso 7.9.0.
0 Kudos
Reply

1,949 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Support on Mon Oct 05 17:02:00 MST 2015
Hi npeterson,

NXP can provide a Hard ABI version for LPCXpresso.  Which toolchain are you using?

Best regards,
-NXP Support
0 Kudos
Reply