Hard fault while running "NfcrdlibEx3_NFCForum" example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hard fault while running "NfcrdlibEx3_NFCForum" example

1,722件の閲覧回数
lucadici
Contributor I

Hi all,

I'm using PN512 with LPC1766. I have ported to my board all the projects belonging to the nxp reader library demo app set (e.g. NfcrdlibEx2_AdvancedDiscoveryLoop).

All of them works fine, except for example "NfcrdlibEx3_NFCForum". Even if I disable both SNEP client and SNEP server and I don't interact with cards or smartphones, running the example results in a Hard-Fault of the MCU.

A strange symptom is that at a certain point the stack seems to detect a card:

/////
 NFC Forum Example:
 
 Multiple technology detected:
     Type A detected...
     Type B detected...
    Resolving selected technology

/////

But actually no activators/targets are in proximity of the antenna!

Is this a known issue for anybody?

#BUG‌

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,482件の閲覧回数
lucadici
Contributor I

The NFC reader library version I'm using is v4.040.05.011646

0 件の賞賛
返信

1,482件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Luca Dici,

Actually this library is designed for lpc1769, so if you changed it to lpc1766, there should be changes in BSP files for lpc1769, if this issue is still there after you change the MCU settings as below:

pastedImage_1.png

you might have to ask help from the lpc community: LPC 


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信