HTTP Request on lpc1768

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HTTP Request on lpc1768

2,618 次查看
navidansari
Contributor III

hi

I have lpc1768 and  DP83848CVV  as Ethernet PHY

I want to send HTTP request to lpc1768

till now I open port and send and get TCP socket and I have a web page that showing simple text

what should I do to be able to get and process HTTP request ?just point me in a right direction or right documentation

the example that exists is old and I can't use it 

标签 (1)
0 项奖励
回复
3 回复数

2,356 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Navid,

Which old example are you referring to? I would recommend you to use as reference the latest available LPCOpen 2.10 package, in specific the webserver example:

LPCOpen Software for LPC17XX|NXP 

If you are using MCUXpresso the LPCOpen package is already included in the installation:

pastedImage_3.png

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复

2,356 次查看
navidansari
Contributor III

im using keil 

0 项奖励
回复

2,356 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Navid,

Then you should download this package:

pastedImage_1.png

 

Hope it helps!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复