HS - ADC, rare signal observed.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HS - ADC, rare signal observed.

714件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rodri on Wed Apr 27 10:40:53 MST 2016
Hi,

I'm sampling a ramp signal with 50% of simmetry, but when I pass it to the PC and plot it with matlab I observe a rare signal.

(attached the images)

As you can see the triangular shape (that corresponds to the one I'm sampling) seems to be the envelope of a faster ramp. This second ramp has a positive pendent when the triangular signal is increasing the value, and negative when the triangular is going low.

Anybody have an idea about what is hapening?

thanks in advance

Regards,
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

704件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

704件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rodri on Mon May 02 14:22:50 MST 2016
Ok, solved.

I thought that was a endian problem or that the bits did not have the proper order, but the problem was in my transfer to pc code... repeating samples in transmission, a stupid error!!

0 件の賞賛
返信