HS - ADC, rare signal observed.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HS - ADC, rare signal observed.

718 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rodri on Wed Apr 27 10:40:53 MST 2016
Hi,

I'm sampling a ramp signal with 50% of simmetry, but when I pass it to the PC and plot it with matlab I observe a rare signal.

(attached the images)

As you can see the triangular shape (that corresponds to the one I'm sampling) seems to be the envelope of a faster ramp. This second ramp has a positive pendent when the triangular signal is increasing the value, and negative when the triangular is going low.

Anybody have an idea about what is hapening?

thanks in advance

Regards,
标签 (1)
0 项奖励
回复
2 回复数

708 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复

708 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rodri on Mon May 02 14:22:50 MST 2016
Ok, solved.

I thought that was a endian problem or that the bits did not have the proper order, but the problem was in my transfer to pc code... repeating samples in transmission, a stupid error!!

0 项奖励
回复