HID USB ROM Driver LPC11U24

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HID USB ROM Driver LPC11U24

1,112 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tanyashir on Wed Jan 30 12:35:12 MST 2013
Hello!

I use HID USB ROM Driver of LPC11U24. I have download examples archive from this link: http://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc11uxx-peripherals-using-lpcxpresso and I have used example named  “USB_ROM_HID” from archive.

This example works. But there is a problem that it sends data with specified intervals. Even if I write zero size of sending bytes to the endpoint, the report goes to the computer, in which the number of bytes is zero.

How can I do so that data are sending only when I need it?
标签 (1)
0 项奖励
回复
0 回复数