HID USB ROM Driver LPC11U24

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HID USB ROM Driver LPC11U24

1,111 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tanyashir on Wed Jan 30 12:35:12 MST 2013
Hello!

I use HID USB ROM Driver of LPC11U24. I have download examples archive from this link: http://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc11uxx-peripherals-using-lpcxpresso and I have used example named  “USB_ROM_HID” from archive.

This example works. But there is a problem that it sends data with specified intervals. Even if I write zero size of sending bytes to the endpoint, the report goes to the computer, in which the number of bytes is zero.

How can I do so that data are sending only when I need it?
Labels (1)
0 Kudos
Reply
0 Replies