[HELP] LPC43S70 developer board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[HELP] LPC43S70 developer board

1,704 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yuuta_togashi on Tue Apr 12 08:46:58 MST 2016
Is there any developer board for LPC43S70. I need a high speed USB and 12 bits ADC to create a DAQ, but I couldn't find any developer board with these characteristics. LPC43S70 has these characteristics, but when I looking for the developer board for this device they redirect me to LPCXpresso43S37, that uses LPC43S37. I'm pretending to buy a developer board and, later, buy the chip and create my own board.
标签 (1)
0 项奖励
回复
3 回复数

1,624 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复

1,624 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Mon Apr 18 02:36:26 MST 2016
Currently there is no development board avialable for the LPC43(S)70, only the Link2 board with the LPC4370 in 100BGA package exists.
Up to now there is no plan from NXP side to create a new evaluation board for especially this chip type.
3rd party eval board manufacturers might take this as an opportunity  ;-)

Which doesn't mean that this chip is no longer relevant for NXP, we produce and sell it under our longevity program:

http://www.nxp.com/about/technology-leadership/product-longevity/product-longevity-nxp-lpc-microcont...

Regards,
NXP Support Team
0 项奖励
回复

1,624 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mysepp on Tue Apr 12 12:29:18 MST 2016
Perhaps

https://www.lpcware.com/lpclink2

Perhaps exchange chip to "S" version by your own?
Check if it offers all pins you need, but I never used it myself, so can't tell if it fits your needs.
0 项奖励
回复