Grouped External Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Grouped External Interrupt

1,390 Views
cleonbrown
Contributor I

I am using LPC1833 Gruop Interrupt, I have 16 external interrupt spread across 2 ports (port 5 and 2) grouped into in one group (GROUP 0). They are pullup resistors on all 16 inputs and it works fine; however, if there is a bad input that pull any of the input low it prevents the microcontroller from getting additional interrupts on the remaining pins regardless of their state.

is this a limitation of the group interrupt?

Please see code below:


void Configure_GroupInt_GpIOs(void)
{
      uint8_t i;

      for( i=0; i <= 15 ;i++ )
      {
            if(i == 7)
            {
                  Chip_GPIO_SetPinDIRInput(LPC_GPIO_PORT, 5, 12);
                  Chip_GPIOGP_SelectLowLevel (LPC_GPIOGROUP, 0, 5, 1 << 12);
                  Chip_GPIOGP_EnableGroupPins(LPC_GPIOGROUP, 0, 5, 1 << 12);
            }
            else
            {
                  Chip_GPIO_SetPinDIRInput(LPC_GPIO_PORT, 2, i);
                  Chip_GPIOGP_SelectLowLevel (LPC_GPIOGROUP, 0, 2, 1 << i);
                  Chip_GPIOGP_EnableGroupPins(LPC_GPIOGROUP, 0, 2, 1 << i);
            }
      }
      Chip_GPIOGP_SelectOrMode(LPC_GPIOGROUP, 0);
      Chip_GPIOGP_SelectEdgeMode(LPC_GPIOGROUP, 0);

      /* Enable Group GPIO interrupt 0 */

      NVIC_EnableIRQ(GINT0_IRQn);
}

Labels (1)
0 Kudos
Reply
1 Reply

1,261 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Cleon Brown,
Thank you for your interest in NXP Semiconductor products and
the opportunity to serve you.
Actually, I'm not clear on the below statement, and I was wondering if you can explain and show me the testing result.

however, if there is a bad input that pull any of the input low it prevents the microcontroller from getting additional interrupts on the remaining pins regardless of their state.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply