Graphical OS installation on lpc1768

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Graphical OS installation on lpc1768

2,517件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by engineer1 on Sat Mar 01 09:01:22 MST 2014
hi
The microcontroller lpc1768 is a graphical operating system installed?
If there,how?
thanks 8-)
ラベル(1)
0 件の賞賛
返信
6 返答(返信)

2,324件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sun Mar 09 11:49:37 MST 2014
Do your own research

http://www.uclinux.org
0 件の賞賛
返信

2,324件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by engineer1 on Sun Mar 09 11:18:41 MST 2014
uclinux is how?
What are its applications?
How did the programming?
thanks
0 件の賞賛
返信

2,324件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sat Mar 08 10:29:05 MST 2014
No, it is not possible to run Linux, android or any other full blown operating system on an LPC1768. You can run ucLinux.
0 件の賞賛
返信

2,324件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by engineer1 on Sat Mar 08 05:59:29 MST 2014
Does anyone have any information about this? 8-)
0 件の賞賛
返信

2,324件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by engineer1 on Mon Mar 03 00:01:23 MST 2014
hi
My question about graphical operating systems such as Android and Linux.
Is it possible on the lpc1768?
thanks
0 件の賞賛
返信

2,324件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Sat Mar 01 09:05:00 MST 2014
Hi engineer1,
Not sure exactly what you are asking,  For your information, you can use emWin graphics S/W with LPC1768 see below BSP.as an example.
http://www.lpcware.com/content/nxpfile/nxpemwin514mcb1700bsp
0 件の賞賛
返信