Gpio based sensor integration in lpc11xx platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Gpio based sensor integration in lpc11xx platform

2,123件の閲覧回数
lofnakumari
Contributor I

Hi,

I gone through the below thread and need the same code required for lpc11u6x. Is this code is working.. Can I have full code of this using this sensor.. wait function is missing.. Plz share the full source code from this thread.. https://community.nxp.com/message/782439#comment-782329

Rgds

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,040件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Lofna Kumari ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
1) Can I have the full code of this using this sensor?
I'm afraid to find the full code, as this thread is migrated from the older community and its server already closed.

Have a great day,
Ping

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,040件の閲覧回数
lofnakumari
Contributor I

please help me the logic if anyone did the same.

Regards

0 件の賞賛
返信

2,040件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Lofna Kumari ,

Thanks for your reply.
To implement it, first, you should understand then transmit protocol by reviewing the datasheet of the sensor, next, manipulate the GPIO implement the transmission according to the protocol.

Have a great day,
Ping

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信