Getting started with nxpusblib

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Getting started with nxpusblib

1,457件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mshrestha789 on Sat Apr 19 09:23:28 MST 2014
Hello friends,

I want to use nxpusblib. I have gone through the examples. I don't have any standard board listed in the examples, so I want to use only usb library i.e. LPCUSBLib. 

In the example I couldn't find where the constants like USB_HOST_ONLY or LPC_43xx is defined.

I am new to this, so please help me regarding this.

Any help will be highly appreciated.

ラベル(1)
  • USB

0 件の賞賛
返信
1 返信

1,447件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Fri Apr 25 14:21:58 MST 2014
Those two constants are not defined in the code, they are only referenced. They are only defined in the compiler's project files.
0 件の賞賛
返信