Getting started with emwin 5.20

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Getting started with emwin 5.20

1,310 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tcmx on Sat Jul 13 20:15:05 MST 2013
Is there any getting-started information on using emWin in LPCxpresso, with boards that don't have an LCD on them? All the existing emWin BSPs are for dev boards that already have an LCD, so they skip over the process of configuring the library and setting up a new emwin project. Essentially, I want to start an emwin project in LPCxpresso, from scratch. If it helps, I'm working with the LPC1114 and an ILI9325-based screen.
标签 (1)
0 项奖励
回复
1 回复

1,234 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Wouter on Mon Jul 15 02:42:12 MST 2013
Hi tcmx,

You may want to check out our start-up guide and our porting guide

Please note that due to the emWin library compile-time settings the memory footprint may be too big for the LPC1114. See: http://www.lpcware.com/content/forum/emwin-high-resource-usage

Regards,
Wouter
0 项奖励
回复