GPIO status after startup during poweron LPC11xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO status after startup during poweron LPC11xx

921件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cjmjansen on Wed Jun 29 01:45:13 MST 2011
When will the gpio input during/after powerup?
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

910件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DiligentMinds.com on Thu Aug 30 18:38:07 MST 2012
All of the IO pins that are configurable GPIO's are configured by default as inputs with a pull-up while a reset is active-- and they will stay that way until you program them to do something else.  There is a power-on reset that is generated internally in the chip, so the GPIO's will be in their default configuration (as above) when the chip is first powered on.

--Ken
0 件の賞賛
返信

910件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vitah on Tue Jul 12 20:02:43 MST 2011
Hi cjmjansen,

Can you explain your question with more detail?
0 件の賞賛
返信