GPIO pin interrupt in LPC 1837 is not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO pin interrupt in LPC 1837 is not working

964 Views
ponalagappan
Contributor III

Hi,

I am trying to use GPIO PIN interrupt in  lpc1837. i need active low interrupt. initially i set the GPIO port and pin in PINTSEL0 register and verified its value.

then doing with configuration registers ISEL,IENR and IENF  as follows 

/* enable level interrupt */

LPC_GPIO_PIN_INT->ISEL = (GPIO_PIN_INT_ISEL_PMODE0_Msk |
GPIO_PIN_INT_ISEL_PMODE1_Msk);

/* enable level interrupt */

LPC_GPIO_PIN_INT->IENR = (GPIO_PIN_INT_IENR_ENRL0_Msk |
GPIO_PIN_INT_IENR_ENRL1_Msk );


LPC_GPIO_PIN_INT->SIENR = ( GPIO_PIN_INT_SIENR_SETENRL0_Msk |
GPIO_PIN_INT_SIENR_SETENRL1_Msk );


/* enable active LOW interrupt */


LPC_GPIO_PIN_INT->IENF = 0x00UL;

LPC_GPIO_PIN_INT->CIENF = (GPIO_PIN_INT_CIENF_CENAF0_Msk |
GPIO_PIN_INT_CIENF_CENAF1_Msk );

0 Kudos
Reply
1 Reply

792 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

I'll close the thread, just keep this thread (Could anyone tell me the sequence of operation to be followed in GPIO PIN interrupt in LPC1837 ).
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply