GPIO key hold detection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPIO key hold detection

1,596 Views
kensu
Contributor V

Hi

Does LPC1830 have any special feature for "GPIO key hold" detection?

Normally, we implement the firmware  "Interrupt and timer" or "polling and timer" to detect the "key hold".

Now I use freeRtos with LPC1830, Does any better or easy solutionfor key hold detect?  

Thanks

Ken

Labels (1)
0 Kudos
Reply
2 Replies

1,452 Views
kensu
Contributor V

Hi Kerry

I understood, 

Very thanks for your reply.

Ken

0 Kudos
Reply

1,452 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ken Su,

    Actually, the GPIO key hold is the basic operation method for all the MCU.

   LPC1830 have no special hardware feature for the key hold. You can use the hardware key dithering or the software key dithering.

  You said you implement the interrupt, timer or polling to detect it, actually, in the freeRtos, the method is still the same for the key hold or key dithering.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply