GPIO interrupt delay on LPC 1769

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPIO interrupt delay on LPC 1769

1,744 次查看
romainhuet
Contributor I

Hello everybody,

I'm new here and I have a small problem with the GPIO interrupt ( LPC 1769). I manage to run the "Pinint.c" program, both with rising or falling edge. But i would like to know if it's normal to have a constant 1.5 micro second delay between the edge of my signal and the start of the handler. I just switch on a led in the interruption program and i can see that the led is on 1.5 microsecond after the edge of my signal.

It seems long and i would like to decrease that but it's like it cannot be shortened. What is the reason of that delay? I read that this GPIO is asynchronous so it should be shorter that a microsecond, isn't it?

Sorry for my english, hoping i'm understandable!

Romain

标记 (2)
0 项奖励
回复
1 回复

1,562 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复