GPIO Interrupts on LPC546xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO Interrupts on LPC546xx

1,813件の閲覧回数
andyjackson
Contributor III

Looking at the latest LPC546xx datasheet (2.6) it says in section 7.15.1 GPIO Features that:

* All GPIO pins can be selected to create an edge or level-sensitive GPIO interrupt request

I need to get an interrupt from pin P4.7 but I cannot see how to achieve this. Both the PINT and GINT blocks only appear to function on GPIO ports 0 or 1 and I can't see any interrupt function in the GPIO block.

I'm clearly missing something as the datasheet is quite clear that all GPIO pins can generate an interrupt.

Thanks for any help,

Andy

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,690件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Andy Jackson ,

The P4.7  cannot generate interrupt , both PINT and GINT cannot support it.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信