GPDMA and EMC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPDMA and EMC

1,094件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giomaca on Tue Sep 10 07:15:47 MST 2013
Hi to all!

I'm using LPC1810 for my application.

Now I want to read data from an external SRAM and write those data to another SRAM.
To do this I have to use the EMC module.

I'd like to know if I could use the GPDMA module in order to transfer (read and write) data between external SRAM.

To do this, should I configure the GPDMA with a memory to memory DMA control?

Thanks in advance,
Giovanni.
ラベル(1)
0 件の賞賛
返信
1 返信

1,063件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Sun Oct 06 23:12:25 MST 2013
Hi, Giovanni,

DMA with mem to mem between external SRAM should work.

Thanks,
0 件の賞賛
返信