FreeRTOS in LPC1343

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeRTOS in LPC1343

1,578件の閲覧回数
vishnuprasadpra
Contributor I

Hello,
I have been trying to implement FreeRTOS in my LPC1343, but for each step I'm encountring with a errors. I would like to know whether I can use FreeRTOS is LPC1343 using IAR. If yes what are the steps I should follow.
Thank you

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,394件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi VISHNUPRASAD,

Yes, it is possible to use FreeRTOS, IAR and the LPC1343. I would recommend you to use the freertos_blinky example project as base for your application. The example is part of the LPCOpen package for the LPCXpreso LPC1343 board, you can download it from this link:

LPCOpen Software for LPC13XX|NXP 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信