FreeRTOS+IO with LPC11UXX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRTOS+IO with LPC11UXX

950 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by neilt6 on Thu Jul 25 15:12:11 MST 2013
Just wondering if anybody's had success marrying the LPCOpen LPC11UXX chip drivers with FreeRTOS+IO? I skimmed through the demo project for the LPC17XX chips, but the BSP layer is dauntingly complicated. Without other examples to compare against, I'm not really sure where to start porting...
Labels (1)
0 Kudos
Reply
1 Reply

936 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Thu Aug 15 09:59:48 MST 2013
There is a FreeRTOS example for the LPC11Uxx included in LPCOpen.
You can find it in the following LPCOpen directory:  LPCOpen\lpcopen_v1.03\applications\lpc11xx\xpresso_projects\nxp_xpresso_11u14
Look at the "nxp_xpresso_11u14_freertos_blinky" example.
0 Kudos
Reply