FreeRTOS: Change baud rate with USART_RTOS_Receive

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FreeRTOS: Change baud rate with USART_RTOS_Receive

跳至解决方案
5,225 次查看
mattyoung
Contributor III

I am using USART_RTOS_Send and USART_RTOS_Receive to send and receive data. It works fine (TX and RX) until I need to change the baud rate. It also works fine to change baud rate if I only transmit (no RX). I believe with FreeRTOS I need to first deinitialize the USART, and then re-initialize with the new baud rate. I do the following:

           USART_RTOS_Deinit(&UARThandleFC4);

usart_configFC4.baudrate = 9600;

           USART_RTOS_Init(&UARThandleFC4, &UARTt_handleFC4, &usart_configFC4);

The above work fine if I am only transmitting. However, I also need to receive data periodically. I receive data with the following, run in one of my other tasks:

USART_RTOS_Receive(&UARThandleFC4, recv_buffer, sizeof(recv_buffer), &n);

The above won’t return until it receives the number of bytes it is expecting (I set this to ‘1’ to return after each byte). Characters can arrive at any time, so I need to keep listening for them. If I attempt a ‘USART_RTOS_Deinit’ while USART_RTOS_Receive has been started in a different task (blocked until a character arrives), my program gets stuck here:

                                /* A task can only have an inherited priority if it holds the mutex.

                                If the mutex is held by a task then it cannot be given from an

                                interrupt, and if a mutex is given by the holding task then it must

                                be the running state task. */

                                configASSERT( pxTCB == pxCurrentTCB );

 

I just need some way to change baud rate, so I am open to other approaches. Is there a way to exit USART_RTOS_Receive even though no characters have arrived? Is there a way to change the baud rate without the Deinit/Reinit process?

I am using MCUXpresso v10.3.1

SDK_2.x_LPCXpresso54618 version 2.3.0, manifest version 3.2.0

Micro: LPC54606J256ET180

Thanks

标签 (1)
1 解答
5,051 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Dear Matt,

One workaround of this could be relese the event that is waiting in the receive task. For example, when you want to change the baudrate you could release rxevent:

xEventGroupSetBits(handle.rxEvent, RTOS_USART_COMPLETE);

and below the receive, change the baudrate, this is an example:

error = USART_RTOS_Receive(&handle, recv_buffer, sizeof(recv_buffer), &n);

if(flag_change_baudrate == true){
   USART_RTOS_Deinit(&handle);
   usart_config.baudrate = 9800;
   if (0 > USART_RTOS_Init(&handle, &t_handle, &usart_config))
   {
    vTaskSuspend(NULL);
   }
   flag_change_baudrate = false;
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Let me know if this helps you.

Best Regards,

Alexis Andalon

在原帖中查看解决方案

4 回复数
3,547 次查看
jusisb
Contributor I

This has been bother me for a week. now the solution works. thanks

 

0 项奖励
回复
3,608 次查看
A_M
Contributor III

Hello, I’m post here because I have the same problem, but the workaround doesn’t work for me.

I must call USART_RTOS_Deinit() asynchrony no matter if USART_RTOS_Receive is waiting or not. I can not wait until next receiving char to reinit uart.

I there any solution?

0 项奖励
回复
5,052 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Dear Matt,

One workaround of this could be relese the event that is waiting in the receive task. For example, when you want to change the baudrate you could release rxevent:

xEventGroupSetBits(handle.rxEvent, RTOS_USART_COMPLETE);

and below the receive, change the baudrate, this is an example:

error = USART_RTOS_Receive(&handle, recv_buffer, sizeof(recv_buffer), &n);

if(flag_change_baudrate == true){
   USART_RTOS_Deinit(&handle);
   usart_config.baudrate = 9800;
   if (0 > USART_RTOS_Init(&handle, &t_handle, &usart_config))
   {
    vTaskSuspend(NULL);
   }
   flag_change_baudrate = false;
}‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Let me know if this helps you.

Best Regards,

Alexis Andalon

5,046 次查看
mattyoung
Contributor III

Thanks, that worked!

0 项奖励
回复