Forgotten GINT1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Forgotten GINT1

1,718 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri May 29 04:21:04 MST 2015
In chip.h there's GINT1 / LPC_GPIOGROUP1 missing  :((

#define LPC_GPIOGROUP             ((LPC_GPIOGROUPINT_T     *) LPC_GPIO_GROUP_INT0_BASE)

Solution:

#define LPC_GPIOGROUP[color=#f00]0[/color]             ((LPC_GPIOGROUPINT_T     *) LPC_GPIO_GROUP_INT0_BASE)
#define LPC_GPIOGROUP[color=#f00]1[/color]             ((LPC_GPIOGROUPINT_T     *) LPC_GPIO_GROUP_INT1_BASE)


Group Init / DeInit is initialising both groups, so:

STATIC INLINE void Chip_GPIOGP_Init(LPC_GPIOGROUPINT_T *pGPIO)


should be replaced with:
/**
 * @briefInitialize GPIO group interrupt block
 * @paramNone
 * @returnNothing
 */
STATIC INLINE void Chip_GPIOGP_Init(void)
{
Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_GINT);
Chip_SYSCTL_PeriphReset(RESET_GINT);
}

/**
 * @briefDe-Initialize GPIO group interrupt block
 * @paramNone
 * @returnNothing
 */
STATIC INLINE void Chip_GPIOGP_DeInit(void)
{
Chip_Clock_DisablePeriphClock(SYSCTL_CLOCK_GINT);
}



标签 (1)
0 项奖励
回复
0 回复数