For LPC3250 800x600 LCD emwin library is available

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

For LPC3250 800x600 LCD emwin library is available

1,621件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ravi Teja on Wed May 09 03:49:33 MST 2012
HI

   Can we  get specific files in emwin for LPC3250
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,555件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ravi Teja on Mon May 14 05:23:32 MST 2012
hi
0 件の賞賛
返信

1,555件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ravi Teja on Mon May 14 05:18:45 MST 2012
Hi

Thanks . We are using Keil in super loop mode . I have gone through the document
We are using the LCD 800x600 . For that one how we can come to know the values for these
TOUCH_AD_LEFT
TOUCH_AD_TOP
TOUCH_AD_RIGHT
TOUCH_AD_BOTTOM

How to compute those values
0 件の賞賛
返信

1,555件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Wed May 09 13:59:20 MST 2012
The emWin v5.14 library binaries for the ARM9 can be found here: http://www.lpcware.com/content/nxpfile/segger-emwin-514-libraries-nxp-mcus

We do not currently have a BSP for this part, but there is a porting document at the bottom of the emWin website that can be used to port the current BSP, which is for the EA LPC1788 and three different LCD displays, over to a board with this part.

Which toolchain do you plan to use?
0 件の賞賛
返信