FlexIO equivalent on LPC55

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexIO equivalent on LPC55

4,000 Views
dav1
Contributor V

Are there any equivalent ways of doing what flexio did on the kinetis range.

need to syncronize the DAC of an LPC55 to control a demux/S&H circuit to achieve say 16 outs or more.

 

Thx 

Labels (3)
0 Kudos
Reply
5 Replies

3,991 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

There is no DAC module of LPC55xx.

 

BR

Alice

0 Kudos
Reply

3,987 Views
dav1
Contributor V

Strange, the datasheet says

2x 12-bit 1Msps DAC
1x 14-bit 5Msps DAC

 

 

Regardless, please reply the question on flexio vs achieving the same using SCT

0 Kudos
Reply

3,973 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Dav1,

About the datasheet you mentioned, please share the part number of your chip, I will check .

About "the question on flexio vs achieving the same using SCT", please describe detail what function

 do you want to do with SCT.

 

BR

Alice

0 Kudos
Reply

3,962 Views
dav1
Contributor V

please see my first post that describes the problem

0 Kudos
Reply

3,938 Views
frank_m
Senior Contributor III

An ADC is something quite different from a DAC.

> need to syncronize the DAC of an LPC55 to control a demux/S&H circuit to achieve say 16 outs or more.

To me it is not clear what that is supposed to mean, especially in the context of other vendor's peripheral connection mechanisms.

The ADC peripheral is extensively described in the MCU user manual, including trigger options (timer, external) and transfer options (DMA).