Flashing program to MCB1200 Keil Evaluation Board using JLink

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flashing program to MCB1200 Keil Evaluation Board using JLink

2,023 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rihana N. on Mon Nov 03 00:19:29 MST 2014
Hi,

We are planning to purchase a Keil LPC1227 Evaluation Board - MCB1200  with LPC1227FBD64 for a project. We have a doubt regarding the flashing and debugging of code in this board. Can it be done only using the ULink2 tool?. Or is it possible to flash using JLink as well? We have a JLink available with us. If this is possible then we could avoid purchasing the ULink2.

Thanks,
Rihana
标签 (1)
0 项奖励
回复
2 回复数

1,918 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rihana N. on Wed Nov 05 01:58:29 MST 2014
Hi,
I am using the Keil IDE. Version 5.12. Can it be used with this toolchain?
0 项奖励
回复

1,918 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Nov 03 21:36:38 MST 2014
Which toolchain are you using? Fundamentally, if the toolchain supports your debug probe, then you will be able to use it to flash and debug your target.
0 项奖励
回复