Flashing program to MCB1200 Keil Evaluation Board using JLink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing program to MCB1200 Keil Evaluation Board using JLink

2,000 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rihana N. on Mon Nov 03 00:19:29 MST 2014
Hi,

We are planning to purchase a Keil LPC1227 Evaluation Board - MCB1200  with LPC1227FBD64 for a project. We have a doubt regarding the flashing and debugging of code in this board. Can it be done only using the ULink2 tool?. Or is it possible to flash using JLink as well? We have a JLink available with us. If this is possible then we could avoid purchasing the ULink2.

Thanks,
Rihana
Labels (1)
0 Kudos
Reply
2 Replies

1,895 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rihana N. on Wed Nov 05 01:58:29 MST 2014
Hi,
I am using the Keil IDE. Version 5.12. Can it be used with this toolchain?
0 Kudos
Reply

1,895 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Nov 03 21:36:38 MST 2014
Which toolchain are you using? Fundamentally, if the toolchain supports your debug probe, then you will be able to use it to flash and debug your target.
0 Kudos
Reply