Flashing on Lpc4357 xplorer++ using openocd on External flash memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flashing on Lpc4357 xplorer++ using openocd on External flash memory

1,290件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by praveen.9123 on Wed Jan 22 06:33:34 MST 2014
I have an NGX LPC4357 xplorer++ board. I need to flash executable on External flash memory using openocd command line.
Is there any steps for flashing. If you know can you you please tell me the steps to flash.
ラベル(1)
0 件の賞賛
返信
1 返信

1,240件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Tue Jan 28 18:17:52 MST 2014
While I have not been successful in flashing a custom board myself (yet), I can tell you that others have been able to flash the Hitex board with SPIFI memory using OpenOCD.

You will need OpenOCD 0.8.0, as OpenOCD 0.7.0 have several problems regarding this.
So first step is to build OpenOCD 0.8.0 from the latest git version.

I plan to try it again later, but unfortunately, I'm too busy to look at this at the moment, however, I think you should know that it's possible. Try searching with Google and also try searching on this forum.
0 件の賞賛
返信