Flashing of HEX file in ISP mode without using of flashmagic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flashing of HEX file in ISP mode without using of flashmagic

1,040件の閲覧回数
ratheesht
Contributor II

Hi,

       I have LPCXpresso 54102 LQFP64 Rev A (OM13077) development board & using LPCXpresso_8.1.0_597 IDE.

It is running with Cortex M4 processor at 96MHz.

I want to flash the hex or axf file through ISP mode but i don't want to use flash magic software or any other standard software.

Is there any way to flash the hex or axf file to the board using cmd window or other method?

ラベル(3)
0 件の賞賛
返信
1 返信

920件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Ratheesh T,

I think it's the only way that use another MCU to parse the hex file, then pack the data in ISP communication protocol and transfering the data to the target MCU.

Hope this is clear.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信