Hello,
While programming the last page of LPC80x, we encounter issue. Tried both on MCUXpresso and FlashMagic. Attached the screenshots and test binaries used. Any clue on what could go wrong?
Thanks.
Hi,
Page 510 and page 511 in sector 31 are not available for user code because of the boot block.
Please check User Manual in chapter 4.3.5.
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
 Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
Thanks for the information.
Wish you a great day.
Hello,
- Do you have the same issue in MCUXpresso?
- What erase blocks are you selecting in Flash Magic?
- Could you please show me a snippet of the error your having?
Regards,
Felipe
Hi,
Here are the answers to the questions:
- Do you have the same issue in MCUXpresso?
=> No issue with MCUXpresso while programming. But,
- What erase blocks are you selecting in Flash Magic?
=> In Flash Magic, used "Sectors used by file" option
- Could you please show me a snippet of the error your having?
=> attached.
Thanks and regards.
Hi,
Could you please try by installing the latest firmware. Try to follow the below document.
https://community.nxp.com/docs/DOC-335453
I hope it helps!
Best regards,
Felipe
Hi, it seems the link is unauthorized or does not exist. Kindly let me know. Thanks!
Regards
Hi, we are using LPC LINK2 Debug probe which is based on LPC4370. In this case, is the information on LPC11U35 still valid?
Hello,
Are you using a custom board?
Regards,
Felipe