Flash driver "UnInit" return code: 0x1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash driver "UnInit" return code: 0x1

1,482件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mokler on Mon May 05 07:58:51 MST 2014
Hello,

I have a board lpcexpresso. With LPC11U14

After connecting some LED to pins I can not flash it anymore with the given error

Flash driver "UnInit" return code: 0x1
  Flash driver "UnInit" return code: 0x1
  15: Target error from Commit Flash write
  Flash verify operation failed.

Is there anyway I can do a hard reset? Or erase the flash?

Thank you.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,466件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue May 06 01:38:44 MST 2014
And which pins did you connect to LEDs? If you used any of the debug related pins, then that will certainly cause problems!

Try booting the part into ISP mode before starting your debug session…

http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access

Regards,
LPCXpresso Support
0 件の賞賛
返信

1,466件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by arw on Mon May 05 14:26:59 MST 2014
Hello,
In LPCXpresso you can erase the flash memory by choosing the toolbar item "Program Flash" which has the icon that looks like a QFP chip outline.

Also please see the FAQ here:
http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access

-AW
0 件の賞賛
返信