Flash IAP - LPC804

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash IAP - LPC804

1,850 Views
Dhaya
Contributor III

Hi,

       We are using Flash IAP concept indeed of storing the required data. While configure the driver alone, it works properly with all sectors other than program stored region.

     While we add this concept with the our application project(having size of 29KB), cant able store the data in 30 and 31th sector also. It always read the value of 0.

     Kindly give the solution  to store the data in IAP ROM.

0 Kudos
Reply
2 Replies

1,829 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

1,790 Views
Dhaya
Contributor III
Hi @Alice_Yang
Yeah similar only. I'll share the project I have. Kindly help us to resolve this issue
0 Kudos
Reply