Firmware update using A/B Partion in NXP LPC54s018

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware update using A/B Partion in NXP LPC54s018

1,872 Views
robo_v
Contributor I

We would like to update the micrcontroller firmware. Can we separate the the flash to A& B partion and NXP LPC54s018 can switch Partion A or B for boot?

0 Kudos
Reply
5 Replies

1,848 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, tell me more about your application this mean that you already have the bootloader with OTA or not?

If not, the recommendation is using the next one.

MCU Bootloader | NXP Semiconductors

Pavel_Hernandez_0-1725401480738.png

Best regards,
Pavel

 

0 Kudos
Reply

1,840 Views
robo_v
Contributor I
Using ISP mode we are downloading the secondary bootloader to RAM and then we are updating the fw image to flash. But in this case,
If the update process did
not finish correctly it can be difficult to recover the old image. So we are looking A/B partion approach
0 Kudos
Reply

1,819 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, just to be clear on what means A/B, are you looking for the OTA process or the recovery image?

Could you elaborate further about?

Best regards,
Pavel

0 Kudos
Reply

1,798 Views
robo_v
Contributor I
Yes Am looking for OTA process of updating the uC firmware. During this process even if it is interrupted or stoped in the middle it should not result in the brick/non-responsive state
0 Kudos
Reply

1,778 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport
0 Kudos
Reply