Firmware Upgrade Over UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Firmware Upgrade Over UART

2,495件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by milind.mishra on Wed Apr 08 01:57:27 MST 2015
Hi,

Is there a utility by NXP which can do firmware upgrade over UART. What I am looking for is something akin to DFU-Sec which should be able firmware but using UART.

Thanks and Regards,
Milind.
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,287件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Thu Apr 09 17:58:58 MST 2015
The flash magic might really help you. Look for the devices under "External Flash".
0 件の賞賛
返信

2,287件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by milind.mishra on Wed Apr 08 04:46:36 MST 2015
Hi Capiman,

Flash Magic can program only On-Chip Flash whereas what I am looking for is a tool that can program the NOR flash connected via SPIFI interface. Not sure whether Flash Magic is capable of doing that.

LPCScrypt is almost similar to DFU-Sec but Firmware Upgrade over DFU is not something that I want.

In short, what I am looking for is a utility that can allows me to transfer the firmware image via UART and then write the NOR flash using SPIFI.

Regards,
Milind.
0 件の賞賛
返信

2,287件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Wed Apr 08 02:20:35 MST 2015
Look here:
http://www.lpcware.com/LPCUtilities

Have a look for FlashMagic or perhaps LPCScrypt.

0 件の賞賛
返信