FatFs performance issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FatFs performance issue

1,347 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jonas2 on Wed Jul 02 04:13:17 MST 2014
Hi,

I use FatFs R0.09 on a Cortex M3 microcontroller (LPC1778) in a multitask environment
(Crossworks tasking library).
I've noticed that some FatFs functions take a lot of time executing, e.g.

f_open:     40 ms
f_close      7 ms

Is this what I should expect or can I somehow decrease the processing time these functions "consume". The clock is running @120MHz so there is a lot of instructions needed for these functions.
One solution would be to open all files at startup and never close them so I only need to use f_write and f_read but I'm not sure if that is a correct way to use FatFs. Have anyone used FatFs like that?

Otherwise FatFs works perfectly.

Thanks!

Jonas
标签 (1)
0 项奖励
回复
0 回复数