Fastest way to learn LPC17xx MCU CMSIS library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fastest way to learn LPC17xx MCU CMSIS library

4,004 Views
hosseinef
Contributor II

Hello every body

i want to know the best way to learn programming for LPC17xx MCUs.

best regards

Tags (2)
5 Replies

3,524 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi hossein ef,

    I also attach the CMSIS library for LPC177X and LPC178X, you can refer to it, this package already have the according help documents which contains all the function.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,524 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi hossein ef,

   I send you a LPC175X_6X sample code based on cmsis driver.

   You can learn the code directly, if you have board, you can try to test.

   I think practice is the fastest way to learn it.

   Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,524 Views
hosseinef
Contributor II

Thanks a lot. is there a document which list all function? i mean a reference document.

the second question is that are the functions same for lpc1768 and lpc1788?

0 Kudos
Reply

3,523 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi hossein ef,

   Please check my attached help file, this is the according LPC1700 Peripheral Driver Library Manual.

   This manual list all the function.

    I think there has some function difference between lpc1768 and lpc1788.

   This CMSIS library supported MCU is list as follows:

pastedImage_1.png

  Now, do you need cmsis library for LPC1788?


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,523 Views
hosseinef
Contributor II

Thanksssss. It was so helpfull. :smileyhappy::smileyhappy::smileyhappy:

0 Kudos
Reply