Fastest way to learn LPC17xx MCU CMSIS library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fastest way to learn LPC17xx MCU CMSIS library

4,061件の閲覧回数
hosseinef
Contributor II

Hello every body

i want to know the best way to learn programming for LPC17xx MCUs.

best regards

タグ(2)
5 返答(返信)

3,581件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi hossein ef,

    I also attach the CMSIS library for LPC177X and LPC178X, you can refer to it, this package already have the according help documents which contains all the function.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,581件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi hossein ef,

   I send you a LPC175X_6X sample code based on cmsis driver.

   You can learn the code directly, if you have board, you can try to test.

   I think practice is the fastest way to learn it.

   Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,581件の閲覧回数
hosseinef
Contributor II

Thanks a lot. is there a document which list all function? i mean a reference document.

the second question is that are the functions same for lpc1768 and lpc1788?

0 件の賞賛
返信

3,580件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi hossein ef,

   Please check my attached help file, this is the according LPC1700 Peripheral Driver Library Manual.

   This manual list all the function.

    I think there has some function difference between lpc1768 and lpc1788.

   This CMSIS library supported MCU is list as follows:

pastedImage_1.png

  Now, do you need cmsis library for LPC1788?


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,580件の閲覧回数
hosseinef
Contributor II

Thanksssss. It was so helpfull. :smileyhappy::smileyhappy::smileyhappy:

0 件の賞賛
返信