Fashing problem on LPC55S69-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fashing problem on LPC55S69-EVK

4,140件の閲覧回数
raz3l
Contributor III

Hi there,

I am running some examples from the SDK_2.5.1_LPCXpresso55S69_GCCARMEmbedded for the LPC55S69-EVK related to Trustzone (Secure Faults example). For each example I created my own Makefile with only the strictly necessary source files (.c, .h, .ld, .S) – which I accomplish by exploring the CMAKE build mechanism (dependencies, compiler flags, etc) provided for each example. I am able to compile the Trustzone-based examples without running to any issue, and I already tested them on the board by flashing through a J-link probe and a GDB session (as recommended on the User Guide).

My next step was to create a makefile-based project on MCUXpressoIDE (File->New->New Project->C/C++Project or New C/C++ Project – I tried both the alternatives), since I wanted to use the debugger interface provided by the tool. For both secure and non-secure applications I was able once again to build them correctly using my makefile (no issues to link the secure gateway library generated during the build of the secure app).

After this process, I run into a issue while trying to initiate a debug session (I am using the on-board debugger). I simply flash the NS app using the LinkServer and once I try to debug the secure app (which I already loaded with the non-secure symbols) I run to an error while the probe is trying to flash:

“Target error from Commit Flash write: Em(12). Target rejected debug access at location 0x1000A000
GDB stub (crt_emu_cm_redlink) terminating – GDB protocol problem: Pipe has been closed by GDB.”

I should add the steps that I took to start the debug session where:

1) Force the LPC555S69 into ISP mode and use GUI Flash Tool to do a Mass Erase".

      Confirmation message: "Operation Complete"

2) Program NS project, by reconnecting first the board debug port.

      Confirmation message: "Operation Complete"

      Console: "Finished writing Flash successfully"

3) Kill active debug session by pressing "Clean up debug" button

4) Edit the secure debugger script and add the command "add-symbol-file <location>TZ_Secure_Faults_NS.elf 0x00010000

5) Debug the secure app and run into the aforementioned error

This is the full debug output:

https://codeshare.io/axEgPd 

I should mentioned that the memory on project settings was the layout of the example provided in the SDK which is intended for the toolchain MCUXpresso IDE (SDK_2.5.1_LPCXpresso55S69_MCUXpressoIDE):

Do you have any idea what step or mistake can I be doing? You can find the resources for the projects attached. 

Makefile (secure): https://codeshare.io/5eLVyr

Makefile (non-secure): https://codeshare.io/adlwrR

Linker Script (secure): https://codeshare.io/anMzWj

Linker Script (non-secure): https://codeshare.io/G8opjd

ラベル(1)
3 返答(返信)

3,767件の閲覧回数
raz3l
Contributor III

Hi soledad‌ and brendonslade‌, thank you for the tips! On the last week or so I have been using MCUXpresso IDE V11, which solve my problems and significantly increased the stability on my development environment! Thanks!

3,767件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

Could you please try using MCUXpresso SDK 2.6 version? 

Older version of MCUXpresso IDE and/or SDK will have different and inferior performance when used with Trustzone examples and are therefore not recommended.

Please check the following document. 

https://community.nxp.com/community/mcuxpresso/mcuxpresso-ide/blog/2019/06/12/using-lpc55s69-sdk-tru...

Have a great day,
Sol

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,764件の閲覧回数
brendonslade
NXP TechSupport
NXP TechSupport

Also be sure to update to MCUXpresso IDE V11. There were several improvements added to this IDE release, including special handling of linked secure/non-secure projects. If you are constructing your own make files and GDB setup this could get more difficult ...

We also just created a new class about secure/non-secure debug; materials are here:

https://community.nxp.com/docs/DOC-343688

I cant see the hands-on lab there so have attached it here.

0 件の賞賛
返信